hi, I’m facing a problem with modem RN-41
the first problem that when i connect Vcc(3.3v) to the modem and measure the volt i find it 1.68 v
i don’t know why this voltage drop occur
you can find my connection in this url http://i64.servimg.com/u/f64/11/34/70/98/untitl11.jpg
is any thing wrong or missed ?
the second that when i apply logic 1 (5v) to max232 it gives -6v
and when apply logic 0 (0v) i get +6v, although pc voltage -12/+12
so is the pc will understand -6 as logic 1 instead of -12
and +6 as logic 0 instead of +12
note that i’m using level converter to convert from 5v TTL coming from max232 to 3.3v for modem RxD