Hi,
I am working on a research project for work where I need to record positional data from a rover. I was looking at the two devices GPS-19984 and GPS-20000, and I’m leaning towards the GPS-20000.
I have a couple questions regarding both devices and was hoping to get some answers.
GPS-20000
- I noticed that this devices comes with 12-months of the correction subscription. If the subscription lapses and I do not renew for the $500, will I still be able to use the device in GNSS Positioning Mode without RTK fix? I understand it’s limited to 30cm accuracy, but I’m curious what kind of accuracy I can expect if the subscription lapses.
GPS-19984
-
For RTK Fix, I am under the impression that I’ll need a reference station to get within the 1.4 cm range. Can I use two of these GPS-19984 devices; one as a reference, and the other on the rover?
-
If I can use two of these in the situation outlined. Can I read the positional data of the rover from the reference station location via serial? For example; I have one GPS-19984 as a reference station next to my laptop, and I have an additional GPS-19984 on my rover. Can I read the rover’s positional data from a direct serial connection to the reference station?
Thank you in advance!