I have a personal project that I need much help with regarding the code necessary to control the LED matrix.
I am hoping to learn the code to create some simple displays.
To have random flowing color changes from top to bottom and also left to right and opposite directions.
I have no knowledge of writing code and I cannot find any suitable examples online.
Most things I find are for 8x8 or 16x32 and a couple for 32x32 but they do not function.
Also I would like to create and display small graphics or icons.
I do not know what lines of code control any function like color, speed, loop etc.
I have an Arduino Mega 2560 and also a Beagle Bone Black A5A development board.
I cannot figure out the pin out for the BBB so I went to the Arduino.
Any help is appreciated.
The LED matrix is a 32x64 P2.5 SMD2121 160x80 1/16S
Item
P2.5
Chip
Epstar
Chip size
Red 9 mil, Green 12. Blue 12mil
Light type
SMD
Pixel Pitch
2.5mm
Module Size
160mmX80mm
Module Resolution
64 X 32 (dots)
Density of pixel
160000dots/m2
Pixel configuration
1R1G1B
Red wavelength
625±2nm
Green wavelength
525±2nm
Blue wavelength
470±2nm
Colors
16777216
Best viewing distance
≥2m
viewing angle
120°/90°
Maximum power consumption
17W
Brightness
2000cd/m2
Gray scale
14bits per color
Color temperature
6500k
Control method
Synchronization or Asynchronization
Driving method
1/16 scanning
Frame frequency
60Hz
Refresh frequency
≥600Hz
Working Voltage
DC5V
IP grade
IP54
MTBF
More than 8000hours
Life Span
80,000hours