I got a couple of the Qwiic Boost (SPX -17238) to help me connect the Sensirion Particulate Matter Sensor - SPS30 which requires a 5V power input. The description for the qwiic boost says:
For applications where the 5V device needs 5V I2C signals, a conversion circuit is provided with the board. A jumper is available to select between 3.3V (default) and 5V I2C signals.
I can’t seem to find that jumper. Support says its on the back but I really can’t find it !
Also want to verify if the qwiic boost has an onboard pull-up resistor (10K), which the SPS30 also needs ?
@YellowDog - Do i have to modify both jumpers in this case or just the one labled “signal level”?
@TS-Russell - thanks for the guides. I guess I will learn something new by doing this. But you didnt say if the boost already has an inbuilt pull up or if I need to use an external one ?