ohh thanks
yes i have the source code library, can you show me what i must change?
/
* LCD driver routines
CodeVisionAVR C Compiler
(C) 1998-2004 Pavel Haiduc, HP InfoTech S.R.L.
*/
#asm
.equ __lcd_direction=__lcd_port-1
.equ __lcd_pin=__lcd_port-2
.equ __lcd_rs=0
.equ __lcd_rd=1
.equ __lcd_enable=2
.equ __lcd_busy_flag=7
#endasm
#pragma used+
static unsigned char _base_y[4]={0x80,0xc0};
unsigned char _lcd_x,_lcd_y,_lcd_maxx;
#pragma used-
static void _lcd_delay(void)
{
#asm
ldi r31,15
__lcd_delay0:
dec r31
brne __lcd_delay0
#endasm
}
void _lcd_ready(void)
{
#asm
in r26,__lcd_direction
andi r26,0xf ;set as input
out __lcd_direction,r26
sbi __lcd_port,__lcd_rd ;RD=1
cbi __lcd_port,__lcd_rs ;RS=0
__lcd_busy:
#endasm
_lcd_delay();
#asm
sbi __lcd_port,__lcd_enable ;EN=1
#endasm
_lcd_delay();
#asm
in r26,__lcd_pin
cbi __lcd_port,__lcd_enable ;EN=0
#endasm
_lcd_delay();
#asm
sbi __lcd_port,__lcd_enable ;EN=1
#endasm
_lcd_delay();
#asm
cbi __lcd_port,__lcd_enable ;EN=0
sbrc r26,__lcd_busy_flag
rjmp __lcd_busy
#endasm
}
static void _lcd_write_nibble(void)
{
#asm
andi r26,0xf0
or r26,r27
out __lcd_port,r26 ;write
sbi __lcd_port,__lcd_enable ;EN=1
#endasm
_lcd_delay();
#asm
cbi __lcd_port,__lcd_enable ;EN=0
#endasm
_lcd_delay();
}
void _lcd_write_data(unsigned char data)
{
#asm
cbi __lcd_port,__lcd_rd ;RD=0
in r26,__lcd_direction
ori r26,0xf0 | (1<<__lcd_rs) | (1<<__lcd_rd) | (1<<__lcd_enable) ;set as output
out __lcd_direction,r26
in r27,__lcd_port
andi r27,0xf
ld r26,y
#endasm
_lcd_write_nibble(); //RD=0, write MSN
#asm
ld r26,y
swap r26
#endasm
_lcd_write_nibble(); //write LSN
#asm
sbi __lcd_port,__lcd_rd ;RD=1
#endasm
}
/* write a byte to the LCD character generator or display RAM */
void lcd_write_byte(unsigned char addr, unsigned char data)
{
_lcd_ready();
_lcd_write_data(addr);
_lcd_ready();
#asm
sbi __lcd_port,__lcd_rs ;RS=1
#endasm
_lcd_write_data(data);
}
static void _lcd_read_nibble(void)
{
#asm
sbi __lcd_port,__lcd_enable ;EN=1
#endasm
_lcd_delay();
#asm
in r30,__lcd_pin ;read
cbi __lcd_port,__lcd_enable ;EN=0
#endasm
_lcd_delay();
#asm
andi r30,0xf0
#endasm
}
static unsigned char lcd_read_byte0(void)
{
_lcd_delay();
_lcd_read_nibble(); // read MSN
#asm
mov r26,r30
#endasm
_lcd_read_nibble(); // read LSN
#asm
cbi __lcd_port,__lcd_rd ;RD=0
swap r30
or r30,r26
#endasm
}
/* read a byte from the LCD character generator or display RAM */
unsigned char lcd_read_byte(unsigned char addr)
{
_lcd_ready();
_lcd_write_data(addr);
_lcd_ready();
#asm
in r26,__lcd_direction
andi r26,0xf ;set as input
out __lcd_direction,r26
sbi __lcd_port,__lcd_rs ;RS=1
#endasm
return lcd_read_byte0();
}
/* set the LCD display position x=0..39 y=0..3 */
void lcd_gotoxy(unsigned char x, unsigned char y)
{
_lcd_ready(); // RS=0
_lcd_write_data(_base_y[y]+x);
_lcd_x=x;
_lcd_y=y;
}
// clear the LCD
void lcd_clear(void)
{
_lcd_ready(); // RS=0
_lcd_write_data(2); // cursor home
_lcd_ready();
_lcd_write_data(0xc); // cursor off
_lcd_ready();
_lcd_write_data(1); // clear
_lcd_x=_lcd_y=0;
}
#pragma keep+
void lcd_putchar(char c)
{
#asm
push r30
push r31
ld r26,y
set
cpi r26,10
breq __lcd_putchar1
clt
#endasm
++_lcd_x;
if (_lcd_x>_lcd_maxx)
{
#asm("__lcd_putchar1:")
++_lcd_y;
lcd_gotoxy(0,_lcd_y);
#asm("brts __lcd_putchar0")
};
#asm
rcall __lcd_ready
sbi __lcd_port,__lcd_rs ;RS=1
ld r26,y
st -y,r26
rcall __lcd_write_data
__lcd_putchar0:
pop r31
pop r30
#endasm
}
#pragma keep-
// write the string str located in SRAM to the LCD
void lcd_puts(char *str)
{
char k;
while (k=*str++) lcd_putchar(k);
}
// write the string str located in FLASH to the LCD
void lcd_putsf(char flash *str)
{
char k;
while (k=*str++) lcd_putchar(k);
}
static void _long_delay(void)
{
#asm
clr r26
clr r27
__long_delay0:
sbiw r26,1 ;2 cycles
brne __long_delay0 ;2 cycles
#endasm
}
static void _lcd_init_write(unsigned char data)
{
#asm
cbi __lcd_port,__lcd_rd ;RD=0
in r26,__lcd_direction
ori r26,0xf7 ;set as output
out __lcd_direction,r26
in r27,__lcd_port
andi r27,0xf
ld r26,y
#endasm
_lcd_write_nibble(); //RD=0, write MSN
#asm
sbi __lcd_port,__lcd_rd ;RD=1
#endasm
}
// initialize the LCD controller
unsigned char lcd_init(unsigned char lcd_columns)
{
#asm
cbi __lcd_port,__lcd_enable ;EN=0
cbi __lcd_port,__lcd_rs ;RS=0
#endasm
_lcd_maxx=lcd_columns;
_base_y[2]=lcd_columns+0x80;
_base_y[3]=lcd_columns+0xc0;
_long_delay();
_lcd_init_write(0x30);
_long_delay();
_lcd_init_write(0x30);
_long_delay();
_lcd_init_write(0x30);
_long_delay();
_lcd_init_write(0x20);
_long_delay();
_lcd_write_data(0x28);
_long_delay();
_lcd_write_data(4);
_long_delay();
_lcd_write_data(0x85);
_long_delay();
#asm
in r26,__lcd_direction
andi r26,0xf ;set as input
out __lcd_direction,r26
sbi __lcd_port,__lcd_rd ;RD=1
#endasm
if (lcd_read_byte0()!=5) return 0;
_lcd_ready();
_lcd_write_data(6);
lcd_clear();
return 1;
}