Hello folks,
I do not understand the meaning of this sentence I found in every QWIIK board’s page:
“As a general rule of thumb, disable all but one pair of pull-up resistors if multiple devices are connected to the bus. To disable the pull up resistors, use an X-acto knife to cut the joint between the two jumper pads highlighted below.”
Here’s an example image.

Which one of the following is true if I have 3 boards connected?
-
I have to cut one of the joints (not two) on every board
-
I have to cut two joints on every board but one (that is, in my case, on two boards out of three)
Thank you!