CAN ANYONE HELP HOW TO HARD RESET EM406-A USING SIRF DEMO SOFTWARE
IS THERE ANY COMMAND THAT SHOULD BE TRANSMITTED TO GPS ???
HELP PLZ
THNKS
CAN ANYONE HELP HOW TO HARD RESET EM406-A USING SIRF DEMO SOFTWARE
IS THERE ANY COMMAND THAT SHOULD BE TRANSMITTED TO GPS ???
HELP PLZ
THNKS
WHY ARE YOU SHOUTING?
Leon
its happened to me a few times. Having blown up the only piece of electronics I had just before the project deadline, then realizing that nothing I do will resurrect it and then going into a state of rage and hate.
may be thats whats happening
ok guys m sorry
can anyone plz tell me how to hard reset EM-406A gps module using sirf demo software
is there any command i should transmit or ???
help plz
try reading this
http://www.navmanwirelessoem.com/assets … alR2.4.pdf
page 2-5 and see if you can send the command to reset to factory settings if that is what you are after. I am assuming the EM-406 is a sirf III that accpets sirf binary protocol
if so you will have to put this into sirf binary command mode before you send the above message