How to receive a bluetooth signal on multiple headsets?

Currently I use the bluetooth on my iphone to transmit music to a wireless headset connected to an amplifier. However, bluetooth cannot connected to more than one headset at the same time. Is there a way to receive a bluetooth signal on more than one headset. Is there a way to override the pairing function or set two receivers with the same pairing code. Or could you split the stereo signal so that two receivers can each receive a mono signal. If there is any way to do this I would really appreciate an answer or if it is pretty much impossible could somebody recommend a good radio transmitter and receivers that could serve the same purpose, preferable of a high frequency to avoid interference. Thanks