How to view library of already existing Eagle Cad files

Hello,

Working on an already existing project that i need to build on. I have the schematic and board files but i need to find out which library they used so i can create a similar board in a new project. is there any way to check which lib was used on the older board and schematic files.

I realize this is a beginner question. any and all responses appreciated.

Kbanner

Using the info button for each component will work, but it’s rather tedious for large projects. Running statistic-brd.ulp or statistic-sch.ulp and saving the report will give you something like the excerpt below.

----------------------------
LIBRARY	Q.
rcl	1   
SparkFun  2	3   
Hirose_usb	1   
pinhead	1   
SparkFun_5.11	1   
FTDI_new	1   

PACKAGE	Q.
C0805	1   
0603-CAP	2   
PTC-1206	1   
UX60SC-MB-5ST	1   
1X03	1   
OSHW-LOGO-S	1   
QFN-16	1   

VALUE	PAC	Q.	Top	Bot
10uF	C0805	1	1	0
0.1uF	0603-CAP	2	2	0
PTCSMD	PTC-1206	1	1	0
USB	UX60SC-MB-5ST	1	1	0
~/-empty-/~JP1	1X03	1	1	0
OSHW-LOGOS	OSHW-LOGO-S	1	0	1
FT230XQ	QFN-16	1	1	0

Jon