Hi, I’ve just received by Weather Station - Weather Meter Kit SEN-15901. Rain and Wind speed are working fine - but having issues with the wind direction. I’ve tried powering directly from my Raspberry PI 3.3v as well as PI 3.3v and then a 10K resistor. And read the return value through a MCP3008. I know the MCP3008 is working properly as I use it for 2 other sensors.
With the wind direction I seem to be getting good values for about 270 degrees of direction, but there is a “dead” zone when I always receive the same value from the MSP3008 through approximately an 90 range.
Is this the appropriate wiring method - should I be using 3.3 or 5 volts? Should I be using a resistor on the voltage, and is so what size. I am assuming it is correct to be measuring the voltage thru the MSP3008, but again tell me if this is wrong.
Thanks and appreciate any suggestions.