Greetings (No Name Supplied),
midnitrcr:
How do you do this in Eagle?
For example… if I have a schematic that takes up a 1x1 space on the board, how can I print 10 copies of these up on one PCB?
The process is called ‘step and repeat’ and it is done to
maximize the use of standard panels used in PCB fabrication.
EAGLE can’t do this for you (there are some clever work
arounds, but these are not for EAGLE beginners).
If you require this process you should look for a
Gerber manipulation tool to assemble copies of
the design files that are output from EAGLE in your
tool chain. Gerbview is popular.
Also, if you submit a single design to BatchPCB that
contains multiple projects (or copies of a single
project) you will have to cut them apart yourself.
This step is called ‘singlation’. The PCBs from
BatchPCB are cut with a router and have nice clean
and straight edges. There should be a gap between
each of your PCB images to allow for the router bit
or saw kerf.
Comments Welcome!