I think i broke my rtk facet

I had to repackage my rtk facet into a waterproof container for an r and d project to use rtk for kitesurfing and snowboarding jump heights. Don’t worry everything was wrapped in kapton tape and double side tape to hold everything in place.

The data collection in vietnam was great and i learned a lot. BUT.

When i got home to oz i re-installed the boards back into the sparkfun case and there is no display. I suspect the display board or connectors based on the forum. I have disconnected the battery and when i press the inside power switch the orange starus led flashes dim then bright then off.

I am coming to the usa next week for 5 weeks. Is there a way i can return the facet and pay for whatever boards i need plus repair costs?

I am about to go through a few of the trouble shooting approaches on the forum. I just want to use the facet as a base station going forward as i just purchased the rtk postcard which has a better form factor for my application.

This post is to confirm i am following the correct diagnosis process and if i need an rma what the process and cost range could be?

Btw i get close to 300mm vertical precision with our local ANZ SouthPAN service. Its a great product.

Sounds like fun!

That’s the right procedure for DIY repair attempts…I presume you’ve seen the manual - and if you’re coming to the US, you have a few options:

  1. Send it for repair now, we ship it to you repaired while you’re in US
  2. Order a replacement panel and replace it yourself
  3. Send it in for repair while in US. We’re in Boulder, CO, and you could drop it off/pick it up at our front counter

Let me know what you think!

Welcome @Ozzieian ! That sounds like a fun R&D :smiling_face_with_sunglasses:

Just incase you didn’t already know this - SparkFun sells development boards also. Take a look at the PostCard if you need to measure the jump heights again in the future. That might be easier than disassembling and reassembling your Facet.

I just bought a full RTK postcard set up. Its form factor is amazing. The only issue is the as shipped version doesn’t seem to support SouthPan SBAS satélite corrections yet. I figure its just a matter of time. Sbas is perfect for many sporting applications.

Ok got off my butt over the weekend and ran a few tests, using the flowchart as my guide.

Firstly batt voltage is fine

Secondly when i press either the membrane switch or the internal switch the orange status led on the main board flashes once dim them once bright then off.

I also tried moving the ribbon cables around but no change in behavior.

It seems like the unit may be working properly but with no display as i was able to connect it to swmaps via bluetooth and it all seemed to be working fine. I did notice it rebooted when i moved it but that may be unrelated

Also my display board uses the old ribbon cable.

Are the display boards available please?

Where to from here please??

Regards Ian


0000000111111111 → 01FF $PQTMCFGSBAS,W,01FF*0F include all enabled
0000000000111111 → 003F $PQTMCFGSBAS,W,003F*7B default enabled
0000000100000000 → 0100 $PQTMCFGSBAS,W,0100*0F only SouthPAN sbas.

$PQTMCFGSBAS,R*27
$PQTMSAVEPAR*5A

Regards

Is it the same cable as in the kit I linked above? SparkFun RTK Replacement Parts - Facet Display/Button - SparkFun Electronics

Yes thats the one, 12 line zif. Does my diagnosis point to screen failure or am on on the wrong track (sic). How do i order that screen as when i last checked it was on backorder? I don’t need a new board juts a working screen for my facet.

Amazing piece of kit for the money.

Thanks ian

Without having it in-hand it hard to tell which is the cause, but the replacement is sold as a set…once one or the other fails we strongly recommend replacing both

DK has 2
Mouser has 1

Then just follow here

I have ordered from dk. It should arrive by the 8th when i get to the USA. If that doesn’t work, i will get an rma and send it to Sparkfun.

Btw i am pretty impressed with the rtk postcard so far but i need to reconfigure it to get southpan sbas.

Regards Ian

I installed the replacement board and screen from digikey and it all works fine again. Thanks.

The sbas correction on the facet is amazingly good tested it in san diego today and getting sub half meter precision after it locks on.

My next project is to configure my postcard to get sbas as well as use my facet as a base station with radio or ntrip to the postcard for my sporting application.

Thanks Ian