Hello,
I am having issues getting my Arduino Uno to recognize the Qwiic Quad Relay through I2C. I have soldered my wires directly to the header pins as I will not be using the qwiic connect. I am using a 5v 4A barrel jack to power the Qwiic board and have soldered the 5V jumper as directed.
Additionally, the SCK on the Qwiic board is wired to A5 on the arduino and SDA is wired t opin A4 on the arduino uno. I have confirmed the board is receiving the 3.3 volts directly at the pin. I haven’t found much support for not using the Qwiic connect and wondered if there is something I should be doing differently. Thank you.