ID-12 with external & built in antenna both work, pos..?

i would like to do this to use my reader on door, having the RFID reader on the inside and the external antenna outside. I hope that i can use two antennas instead of two readers. I was wondering does ID-12 is a capable to energize both antennas.

Does anybody try this?

Thanks

If you placed it inside the door, maybe you could get it to read from both sides… (i don’t have one so i can’t test to see if it can)

I’m holding a big “Experimentation Needed” sign above my head for the rest of this thread… :lol:

I did that with my door. You only need one external antenna that you will put on the outside. The ID-12 chip also has internal antenna that is never disabled, so you have both sides covered:

RFID lock with ID-12 reader and PIC16F84:

http://www.elektronika.ba/498/rfid-lock … -and-id12/

Muris:
I did that with my door. You only need one external antenna that you will put on the outside. The ID-12 chip also has internal antenna that is never disabled, so you have both sides covered:

RFID lock with ID-12 reader and PIC16F84:

http://www.elektronika.ba/498/rfid-lock … -and-id12/

Muris, thank you!

And “www.elektronika.ba” is an excellent base of knowledge in electronics

Hvala jos jednom, ako bude potrebno oko izgradnje ext.antene mogu li te kontaktirati?

No problem, you can contact me if you need any info :slight_smile: