My TOP106 antenna has been powered down for a few weeks while I’ve been tinkering with the ESP32 RTK base and connected GPS-RTK-SMA, and now I’m having problems getting GPS FIX. The unit sees a lot of satellites, but with SNR 0.0 - then it works for a while before it returns to NO FIX. The problem is probably related to a small heap of snow on top of the antenna. The antenna worked well the entire last winter, but I think the first snow this year got frozen onto the surface while it was disconnected. It is possible to remove the snow mechanically, but then I would need to rent a boom lift again.
Is it possible to inject DC current into the antenna (by using a bias tee injector?) or in some other way increase the operating/surface temperature of the unit?