Inquiry About M7E Hecto RFID Modules

(P.S. I initially reached out to the Official Support team about the questions below, and they directed me to you for further help.)

Dear SparkFun Team,

I am a student based in Germany currently working on an automation project involving UHF RFID tags and readers. While researching suitable modules, I came across your website and found the following two products particularly interesting:

ThingMagic M7E Hecto UHF RAIN RFID Module
SparkFun Simultaneous RFID Reader – M7E Hecto
I understand that both products are based on the M7E Hecto module. I would therefore appreciate some clarification on a few technical questions:

Reading Distance:

What reading distance can I reliably expect when using the module without an external antenna? My target is a stable reading range of approximately 1.5–2 meters. Is this realistically achievable without an external antenna?

Difference Between the Two Products:

My understanding is that the SparkFun Simultaneous RFID Reader mainly simplifies development by providing integrated connectors and an easier interface. Is that correct?

If so, would it be possible to integrate the ThingMagic M7E Hecto module onto a custom board and use the same Arduino library provided for the SparkFun reader?

Software Support:

Besides the Arduino library, are there additional software resources or SDKs available?

Also, is the Arduino library compatible with the ESP32 platform?

I also have a few logistical questions:

Shipping to Germany:

What is the estimated delivery time to Germany? As I am working under time constraints, this information would be very helpful.

Return Policy:

If I order the SparkFun Simultaneous RFID Reader and test it carefully (without soldering, only using USB or I2C), would it be possible to return it if the reading range does not meet my requirements?

If so, would I be responsible for return shipping costs, and could you provide an estimate of those costs?

Technical Support:

If I encounter issues with the Arduino library or integration, does SparkFun provide technical support for such cases?

Finally, I noticed the following warning on the product page:

“WARNING: This product may contain chemicals known to the State of California to cause cancer and birth defects or other reproductive harm.”

Could you please clarify what this warning specifically refers to and whether there is any practical safety concern during normal usage?

Thank you very much for your time and support. I look forward to your response.

Kind regards

Don’t worry about that at all, EVERYTHING causes cancer according to the state of California. As long as you don’t eat, liquefy it and drink it, or smoke it, you will be fine. The warning comes from a law in California called Proposition 65, it’s a bit of a joke outside of California.

Reading Distance: 1.5–2 meters. Is this realistically achievable without an external antenna? No…a couple inches at best w/o. But with the right one you can scan a bit over 16 ft away

Difference Between the Two Products: Yep. That’s what a lot of our original products do

Software Support: In addition to the Arduino Library there’s a windows app Using the Universal Reader Assistant - SparkFun Simultaneous RFID Reader - M7E Hookup Guide ; yes esp32 is arduino compatible

Shipping to Germany: You can check rates/estimated dates in the shopping cart

Return Policy: Depends; we have a 30-day return window for most items …yes, you would be responsible for return costs. The main thing is to understand it has a VERY limited range of a few inches without an external high-gain antenna

Technical Support: You’re lookin’ at it :slight_smile: Also, we have guides

I unofficially concur with YellowDog’s post concerning California Prop 65 stuff

some additional remarks.

You mention I2C, that is NOT available on the M7E, only Serial & USB.

You can also connect to a Raspberry PI. There is an extensive library from Jadak / Thingmagic (Mercury API) that can be used. The Sparkfun library is contains a subset, good enough for 80% of reading and writing tags. But when you need to do something special (which I don’t expect for a school project) the Mercury API contains more options.

No need to order in de USA. You can order the M7E reader board from a local distributor. E.g. in the Netherlands for Sparkfun I use Mouser, Digikey or Antratek. The later has the M7E reader in stock, also tags, external antenna and wiring.

When using with external antenna, you will increase the power (e.g. 2700dBM). The M7E will turn hot quickly (make sure to add cooling block) and make sure to have a strong external power supply.

There are many good articles in this forum that contain answers to many questions and issues which can save you a lot of time.

It’s a joke inside of California too.