is SAM BA is copy itself in flash or sram?

hi,i read in the olimex site that:

“When the TST pin is set during power-up and PGMEN0, PGMEN1 and PGMEN2 are set, the device is entering is a specific test mode and performs a SAM-BAâ„¢ Boot System Recovery which consists in copying the SAM Boot Assistant (SAM-BAâ„¢) in the first two sectors of the on-chip Flash memory. The system recovery procedure takes 10s.”

but in datasheet i read that it copy it self in sram & only 8k bytes left for user.

can some one explain it for me?