Setup:
We connected two SparkFun LG290P Quadband GNSS modules through UART3.
From the default values:
- Set the base GNSS to base mode with:
$PQTMCFGRCVRMODE,W,2 - Changed the baud rate of UART3 to 115200 with:
$PQTMCFGUART,W,3,115200
(as we are planning to use the SparkFun LoRaSerial Kit – 915MHz to send the RTK corrections, and the maximum baud rate is 115200).
3.Configure the base station to Survey-in mode
$PQTMCFGSVIN,W,1,60,15.0,0,0,0*3E - The baud rate of the rover has also been changed to 115200.
Each module is connected to a separate antenna.
Current Situation:
The RTK LED is blinking, but we receive the following errors:
- On the base board:
$PQTMVER,ERROR,3 - On the rover board:
$PQTMVER,ERROR,3
Any suggestions?