issues with the Color LCD Analog pins

I am using the Color LCD shield (sku: LCD-09363) with an Arduino Uno board. I am finding that the analog pins on the LCD shield do not provide a clean pass through. I have used a different type of shield and the results are what I expect - clean pass through of the analog signal. So it seems to me to be a problem with the Color LCD shield. The Color LCD shield works properly otherwise. I can display the data I send to it. Also, I have tested the headers that were soldered on and they check out just fine.

Is anyone else having this problem with the analog pins on this shield? I know I could simply snip the lead coming out of the header and plug my analog signal straight into the Arduino board - I am just wondering if I have a bad board. Thanks for the help.