Jumpers on Olimex E2214 board

I am not able to program the flash on my Olimex E2214 board. I am using Philips LPC2000 Flash Utility v2.2.0. The utility just says it’s not able to connect with the board.

I did short the BSL jumper but looks like the other jumper settings are not correct. What should be the proper settings for these jumpers while programming the flash:

DBG

JRST

DLS_EN

BOOT0, BOOT1

And, what should be the serial port baud rate? Thanks.

Use Flash Magic, it’s a lot better than the NXP utility.

Leon

I have an Olimex E2124 and to program using flash utility both jumpers JRST and BSL have to be shorted.

To flash with Linux there is [lpcflash

Edit: [E2214/E2294 Documents](lpc-e2214 user's manual board - SparkFun Electronics Forum)](Google Code Archive - Long-term storage for Google Code Project Hosting.)