Keil and H-JTAG

I want to program STR911FAM42 chip by Keil. I configured keil per instructions: H-JTAG.dll as RDI Interface driver and “STR91xFxx2 Flash Bank 0 ICP” as programming algorithm. RAM for Algorithm is 0x4000000 and the size is 0x0800 (I tried different values as well).

When I hit Download button it says “Cannot Load Flash Programming Algorithm”. However, the ranges R/O base and R/W base matches the algorithms range…

If I use "“STR91xFxx2 Flash Bank 0” not ICP, this time it says "Load size error. (Addr:=0x04000000) in the output pane.

Any ideas?

I could not find any solution to this. And I saw that Keil has many bugs even by the very first clicks of user interface you came across a bug… I really do not understand a product that has been on the marked for a very long time and a big price has this many bugs…

Does Keil software actually support H-JTAG?

Leon

It claims that it supports RDI…

IAR Supports RDI too. Using IAR I can download and run the code using H-JTAG…