I have read the datasheet on this module but cannot find what the actual range (metres) of this transceiver.
i have the power output set to 0 dBm. (there iare -5,-10.-20 and 0 settings available). How does this translate to actual metres?
richt now I’ms truggling to get more than a few metres. However this might ahve to do with my software protocol and the fact that I’m right next to a heavy machines lab.
I have used Laipac’s transmitter and receiver “a few meters” also, but not their transceiver. My experience with the Tx and Rx is about consistent with yours. I could successfully transmit about 50 feet when going through a concrete foundation wall, but the quality of transmission was poor. Probably 30% effective. If I got to within, say, 20 feet, without anything in between, the transmission quailty went up dramatically.
I also was able to get about 200 feet outside on a clear night, and probably could have gotten farther–but without anyone else to tell me if the transmission was successful at the other end I couldn’t tell.
In short, my results are consistent with yours. I believe Sparky has done some range tests (or at least I thought I saw them here at SparkFun), but check out the laipac site as well.
turned the transmission speed to 250k and I got an extra few metres. For some reason I thought these transceivers had ranges approaching 200m. Anyway thanks for the help
200m is the theoretical max based on the sensitivity and power of the Nordic nRF2401 chip. In practice, it’s not that far.
I was able to go 97 steps (truly scientific) before the link with the SMiRF broke down outdoors - line of sight. Add concrete, ovens, domesticated animals, and your viable transmit distance goes down.
I like to recommend the 24G units for ‘same room’ applications. If you can see the computer, you can most certainly communicate with a 24G unit to it.