Does this shipment refer to the one from the PCB fab to BatchPCB, or from BatchPCB to end customers?
The panel for my order is lower than the last panel shipped as indicated by the BpcbStats page, yet I have not received anything yet and my order still shows up as “processing”. Hence my question.
It refers to shipping to BatchPCB to end customers. It’s possible your panel was out of order – maybe it needed redone. Normally there would be an email to you when your board ships to you. I would ask support if I were you.
analogon:
It refers to shipping to BatchPCB to end customers. It’s possible your panel was out of order – maybe it needed redone. Normally there would be an email to you when your board ships to you. I would ask support if I were you.
Thanks analogon. I received the email indicating that my order had shipped. I didn’t have to contact BatchPCB support. I used the cheapest shipping option (first class USPS mail) but even then I got a tracking number that I could use to track the package, so that was nice.
What was confusing to me is that I received the shipping notice email from BatchPCB about a week after “Last panel shipped was nnnn on mm/dd/yy” indicated that my panel had shipped.
Anyway, it’s all good – I now have my PCBs and am very happy with the service. It was a long wait, though, but it was clear based on the BatchPCB FAQ that it was going to be like that.
Indeed, it has increased since my post I’ve also seen panel #1080 for a short time !
It was mainly a question about the update rate of these informations : do they really reflect what is sent ? I think a 1 day delay is not that much, but here there was a complete week without any update.
Edit: Do you know what is the average number of boards/designs per panel ?
There’s something odd about the system. Right now the last panel shipped was 1082 on 10/27/10, but I received my order today and it was on panel 1084 Moreover, my order is still being processed according to the order status page, but there is a tracking number on the page (and the page was last changed on 10/27/10). So I’m guessing that the “last panel shipped was nnn on mm/dd/yy” is not always up to date.
I believe that my four boards were on panel panel 1088 or 1089 or somewhere in that range.
I have yet to receive an email so far. Status is still listed as processing and now the web page states that 1095 has shipped. I also wonder if response is slow. No real issue other than I hope to have them by early next week. It would be nice to have them for my show and tell demonstration next Friday evening.
buckanear7:
I believe that my four boards were on panel panel 1088 or 1089 or somewhere in that range.
I have yet to receive an email so far. Status is still listed as processing and now the web page states that 1095 has shipped. I also wonder if response is slow. No real issue other than I hope to have them by early next week. It would be nice to have them for my show and tell demonstration next Friday evening.
buckanear7:
okay now I understand how to get the panel info. So now where is panel 1091 in the flow of things since 1095 has already shipped? just curious.
james
The “Order Status:” description should tell you that.
I wouldn’t be surprised if sometimes panels do not come in in exact order. Would yours be a 4-sided board maybe? Just a long shot question.
The “Order Status:” description should tell you that.
I wouldn’t be surprised if sometimes panels do not come in in exact order. Would yours be a 4-sided board maybe? Just a long shot question.
No. all four designs are 2 layer. Only thing I would figure is that one board is 1.9 inch diameter in size. Yes it is a round board. :? :? I am hoping it did not cause any trouble.
james
edit comment:
Yes I am aware that 4 layer designs the panels can get out of order.
The size and shape will not cause any problems. Also yes, Panels do ship out of order. Just to clarify “paid” means your order is in line to be panelized. “Processing” means your order has been panelized and is in line to be manufactured. 4 layer orders do NOT get panelized, they are sent out individually.
The size and shape will not cause any problems. Also yes, Panels do ship out of order. Just to clarify “paid” means your order is in line to be panelized. “Processing” means your order has been panelized and is in line to be manufactured. 4 layer orders do NOT get panelized, they are sent out individually.
Thanks for the input. It has been just about 12 business days since the status of “processing” has been on the board.
If they ship by the end of this week, will still be within the window.
Man i was just about to post this exact question…glad i looked first This is good to know, my boards are 5 away from being shipped, means they’re probably en-route from china now.
This is the dates of the panel that we have sent out to the customers. Panels do return out of chronological/numerical order sometimes. I know this can be confusing, but if you ever have a question about your order feel free to email support@batchpcb.com.