I’m seeing that your LIDAR-Lite v4 LED distance sensor uses the nRF52840 microcontroller and that it is designed so that the user can create their own program to run on it. In order to create a custom program I think it would be necessary to have a schematic for the board and it would be super helpful to have an example project that implements the code that currently ships installed. Are these available? I have not been able to find them.
I am a microcontroller expert and have been doing firmware for a long time so I am comfortable creating my own program once I have at least a schematic. (An example project would save a ton of time though.)
Also, in my application I don’t really need the radio stuff. I may be interested in helping to change the design so that you have a non-radio version that is designed for low power applications…