I used SparkFun’s PowerCell (https://www.sparkfun.com/products/11231) in a prototype product and then integrated the circuit onto our main PCB board. It has stopped working after about 4 months of use and I am having a very hard time trying to debug the issue. I just can’t find anything wrong. I think there must be something wrong in my component selection or design - because I had weird issues when I first tried the circuit. I quickly had to replace the chip and it seemed to work fine for several months…
-The battery is fine
-The charger part of the circuit works fine
-I have made very few changes to the original circuit
-There is nothing on the boost chip’s output
-Voltages on all control inputs look fine
-I am reading 4.2V on my USB 5V line when the circuit is activated… This seems strange
-I have never witnessed the main circuit draw over 400ma and I have tested in peak conditions.
Info on the circuit here: https://docs.google.com/document/d/1T1H … momOE/edit
Eagle files: https://drive.google.com/file/d/0ByaeK3 … sp=sharing
https://drive.google.com/file/d/0ByaeK3 … sp=sharing
(first real Eagle project ever…)
I would be so appreciative of any advice - this is driving me crazy.