Hello, [BallSportsGear
I bought the SparkFun LiPo Charger/Booster - 5V/1A to power my project with a single cell LiPo battery. The board is supposed to charge the battery via the micro-USB port and boost the output voltage to 5V. However, I noticed that the board does not charge the battery properly. The charging LED stays red even after several hours of plugging in the micro-USB cable. The battery voltage remains low and does not reach the full capacity of 4.2V. The board also gets very hot during the charging process.
I checked the connections and the polarity of the battery and they are correct. I also tried different micro-USB cables and power sources, but the problem persists. I measured the current drawn by the board and it is only around 100mA, which is much lower than the expected 1A. I suspect that there is something wrong with the PAM2401 IC or the protection diodes on the board.
Is this a known issue with this board? How can I fix it or get a replacement?
Please help me to fix this issue. Any help would be appreciated.
Best regards,
Nicholas185Smith](https://ballsportsgear.com/)