thanks for the quick answer. Indeed, I want to measure pressure and tensile forces alternating during my process without pausing the measurement inbetween.
I want to use the HX771 load cell amplifier and want to connect it directly to a Raspberry Pi. Could you tell me, if this easy mounting is working for measuring tensile and pressure forces without recalibration?
And you wrote that it can depend on the load cell itself. Are there diffeerent type of load cells that are delivered when I order the mentioned one?
The_Questioner:
I want to use the HX771 load cell amplifier and want to connect it directly to a Raspberry Pi. Could you tell me, if this easy mounting is working for measuring tensile and pressure forces without recalibration?
I don’t have any experience with the HX771 but the spec sheet seems to indicate that the input covers the full range positive and negative. Some instruments have a figure like ‘input range: -0.5 to 36 mV.’ Here’s an example: [scale indicator spec sheet. In this example, they give this as 'Analog input signal range: -1 to 5 mV/V. So if you had an S-beam with a 2mV/V response like in your OP, it will only measure to about half capacity in the negative direction.
And you wrote that it can depend on the load cell itself. Are there diffeerent type of load cells that are delivered when I order the mentioned one?
There are some S-beam cells that are specifically tension OR compression. Here are two load cells like this:
I’m unclear on the differences between these two. It could be as simple as wiring differently so that the output always drives positive or the installation of additional hardware like check bolts or overload stops.
Hey, thanks for the specific explanation. I think I got on which paramters it depends. I checked my components regarding your advices and think the process I want to establish should work with it.