logomatic v2

Hi,

I want to connect a Garmin GPS unit to the logger as well as connecting a wind direction and wind speed sensor.

Can these be conected at the same time- wind sensor is a relatively standard unit which has a frequency output for wind speed and variable resistor for wind direction. Both could be converted into analog voltages for input.

Can these be logged at the same time as the GPS data which is in NEMA 1083 format

Thanks

Randal