Looking for a transmitter/receiver switch

I am looking for a transmitter, and receiver that will act as a a switch when +/- 10V is applied to the transmitter, I am looking for a receiver that can turn a device on or off when voltage is applied to the transmitter. Is there a package receiver that can apply “X” voltage/amperage after receiving a signal from a transmitter that transmits after being supplied a voltage? (“X” voltage being low, 10V or less. Not sure what yet, and Transmitting range around 25-50 feet ideally or even more).