I’ve been working with a CC1100 eval board connected to a PIC, and then to a PC via RS232, and have trouble getting a decent link, so my range is bad (I can barely take it out of the room and down a short hallway, even at +10dBm). I’m typically getting ~10-30 for the LQI value. I’m using the register values that SmartRF gives you, so I’m wondering if I’m missing something here… Is there some values you have to tweak? Do I need to do something different to calibrate it other than put it in idle and give it a SCAL command? Any help would be really appreciated, it’s been really frustrating!
Related topics
Topic | Replies | Views | Activity | |
---|---|---|---|---|
Question about X-CTU and LQI (Xbee 24ZB) | 3 | 1446 | June 18, 2010 | |
Range problems with a CC1100 | 6 | 3508 | June 4, 2008 | |
Very cheap, very low bandwidth, very short range wireless | 7 | 1379 | January 22, 2009 | |
TI/Chipcon CC1101 board design - 868 MHz | 43 | 41363 | November 26, 2013 | |
RF Link - 4800bps - 315MHz | 0 | 662 | October 14, 2008 |