hello ı need lpc2378(olimex lpc-p2378 dev.board) timer blink sample for eclipse.
someone help me about this.
regards…
isma
hello ı need lpc2378(olimex lpc-p2378 dev.board) timer blink sample for eclipse.
someone help me about this.
regards…
isma
any ideas :?:
Hellllppp ![]()
void Initialize(void);
void feed(void);
void IRQ_Routine (void) __attribute__ ((interrupt("IRQ")));
void FIQ_Routine (void) __attribute__ ((interrupt("FIQ")));
void SWI_Routine (void) __attribute__ ((interrupt("SWI")));
void UNDEF_Routine (void) __attribute__ ((interrupt("UNDEF")));
void T0isr (void) ;
/**********************************************************
Header files
**********************************************************/
#include "LPC23xx.h"
#include "type.h"
#include "irq.h"
#include "target.h"
#include "fio.h"
int r;
void main (void) {
IODIR0 = 0x00200000; // P0.21 Output
VPBDIV = 0x00000002;
PINSEL0 |= 0x00000000;
T0PR = 0x0000001E;
T0TCR = 0x00000002;
T0MCR = 0x00000003;
T0MR0 = 0x00001600;
T0TCR = 0x00000001;
VICVectAddr4 = (unsigned)T0isr;
VICVectCntl4 = 0x00000024; //4 No int enable (Timer0)
VICIntEnable |= 0x00000010; //Timer 0 int enable
while(1);
}
/******************************************************
Timer 0 interrupt
******************************************************/
void T0isr (void) {
r=(r+1)&1;
if (r==1)
IOSET0 = 0x00200000; /* Turn off LED */
else
IOCLR0 = 0x00200000; /* Turn on LED */
T0IR |= 0x00000001;
VICVectAddr = 0x00000000; //Dummy write to signal end of interrupt
}
/* Stubs for various interrupts (may be replaced later) */
/* ---------------------------------------------------- */
void IRQ_Routine (void) {
while (1) ;
}
void FIQ_Routine (void) {
while (1) ;
}
void SWI_Routine (void) {
while (1) ;
}
void UNDEF_Routine (void) {
while (1) ;
}
where is my fault? ![]()
up