Hi guys,
I bought M6E-Nano board with the USB-serial attachment and some UHF tags.
Following the guide at sparkfun, im trying to simply read the tags. I’ve been trying to use the URA (Universal Reader Assistant) for this, but so far its not working. The URA checks my card, but when setting it to “Read”, it does not catch any tag.
I’ve checked the dbm power below 5dbm (using usb-serial), but right now my concern is the firmware version.
According to URA, only M6E with firmware v1.19.0 and later can be used and Nano firmware must be v1.5.0 and later.
First, I dont understand which firmware should I update? The M6E? or the Nano? I cant seem to find any M6E-Nano firmware on Thingmagic…
Second, when trying to update the firmware thorugh the URA, using the M6E 1.21 update it gives me the following error: “a flash command can not access multiple sectors”. Using the Nano 1.7 update, it gives me a “Succesful” message, but the firmware its still the same…
This is my actual conf according to URA:
-
Firmware Version : 1.07.03.17
-
Hardware Version : 30.00.00.02
-
URA Version : 3.4.34.34
-
Mercury API Version : 1.29.4.34
Can anyone help me with this? Any tips?
Many thanks in advance!