Hello,
I am a happy owner of the above reader, using it with an Arduino and Arduino IDEs serial monitor on Windows 10. It works very well for the big [standard tags in close range 3 - 5 cm. Since I want to use it for a museum installation where I need to simultaneously read (count) the number of up to 20 individual objects close to the reader (up to 0.3 m) I need to increase the range of the reader. When I set the nano.setReadPower(500); it works well but with any higher number (using a wall power plug) like ```
nano.setReadPower(1500);
Ideally, I also would like to read the [[Ultra-Small UHF RFID Tag Rain ](https://www.sparkfun.com/products/16464) in that distance. I guess this won't be feasible with the onboard antenna. Is there any flat antenna which can be installed into a table like furniture to read these tags (the standard or ideally the Rain tags)? Any help appreciated! Many thanks, C.](https://www.sparkfun.com/products/16464)](https://www.sparkfun.com/products/14147)