Hi,
I recently had to switch from Arduino Mega to Due. I was using M8U Ublox module on Mega for a while without any issue using I2C. However, The same layout with Due does not work as expected. I am reading the GPS and IMU data via I2C but It is too slow. It updates every 3 seconds.
I do not have the option to go back to Mega and I have to get this module working properly with Arduino Due.
Not sure what is going on. The code and wiring is 100% identical for both boards but Due does not like it. Even though it is supposed to be the faster board than Mega.
Thanks for the help