Good morning.
I reversed the helical planetary gearbox (https://www.oyostepper.com/category-199-b0-Helical-Planetary-Gearbox.html) to use it as a speed increaser, connecting the low-speed end to the turbine and the high-speed end to the generator. The result was a 10% lower power generation efficiency than calculated, severe overheating of the gearbox, and oil temperatures easily exceeding 100°C.
I suspect that the helical gearbox is operating like a “turbine” during reverse drive, reversing the axial force direction. The bearings that originally bore the thrust are now bearing the reverse tension, leading to a dramatic increase in bearing friction loss.
The thrust bearing wasn’t selected to handle bidirectional forces, and replacing it now is too late.
Could adjusting the oil viscosity temporarily alleviate the problem, or could an auxiliary thrust disc be temporarily installed to share the reaction force?