Dear community,
I need for my project a 7.4v supply (in order to successfully power a thermal printer and other devices). My device has to work both on battery, and on USB +5V wall power while it is being charged - it should not power off. In my personal stock I have 2x3.7v (10.000mAh) batteries, 2 Sparkfun battery babysitters and also a 2S balanced charger module.
What I tried so far:
- 
Output batteries in parallel and use a step-up module (https://www.pololu.com/product/2570) to get the required voltage: stepper ups don’t seem to source enough power (?) so the thermal printer will not run.
 - 
Output batteries in series, using balanced charging modules, but it seems like only one battery is discharging and not charging up completely. The balanced modules are this:
 

Now, my final try was using the Sparkfun battery babysitter (love those modules). So I build this setup:
Now, sorry for my limited electronics knowledge, but this is what happened:
- The setup provides 7.4v, but only if i do not connect the supply (dotted) lines. Once I do this, all grounds are the same, and one module will be shorted (I think) and leds turn off. So I said, ok i will add some diodes on the negative terminals on the supply lines and this sort of worked, but only as long as I do not plug in a 5v supply. Once I plug in a 5v supply, only one babysitter is firing the charging led (and charging its battery).
 
Any advice would be of great help. Thank you very much!
George