Maximum Update rate for NTRIP enabled with SparkFun GPS-RTK-SMA Kit

I’m thinking about buying SparkFun GPS-RTK-SMA Kit. SparkFun GPS-RTK-SMA Kit

Q1: What will be the maximum update rate when NTRIP is enabled using 4G network?

Q2: And is there any documentation of NTRIP credential input?

Q3: What extra modules do I need to buy to use my Android smartphone to collect cm-level accuracy data? And, Are there any tutorials or documentation available for integration with android phone?

Does it need a High Rate? Are you doing anything that would warrant >1Hz ?
The ZED’s have a 2 minute timeout on RTCM3 aiding, what’s critical is maintaining carrier-lock once you have ambiguity resolved on each of the signals.

I need a better update rate >10Hz

You can likely find tutorials if you look…
Here’s on from ArduSimple, but the method/mechanics are going to be the same

Thanks, I have already looked at their modules also.

I need a better update rate >10Hz

For NTRIP, I seriously doubt it. it’s aiding data, the carrier behaviour at a static base isn’t remotely dynamic enough to need a rate matching the SOLUTION rate.

Multi-constellation on the ZED-F9P the RTK Solution rate is perhaps ~7 Hz max, higher for GPS Only

Umm, got it. Using just this module simpleRTK2B – Basic Starter Kit will I be able to connect on my Android device using OTG cable?