Hi,
the last few months I was testing different MEMS Microphones in breakout Boards in an ultrasonic surrounding (up to 120 kHz). I found that the frequencies could be measured correctly with several MEMS Microphones. However, the ultrasonic Signal is too strong at lower frequencies (around 25 kHz) so that the MEMS-Signal starts to clip (I used only analog MEMS).
I think the solution for this might be, to use a MEMS Microphone with an lower sensibility (around -50 dBV?).
The VM2020 Breakout Board you were offering seems perfect for me. Unfortunately this MEMS isn’t produced anymore. ![]()
Do you have an similar Breakout Board or any MEMS you can suggest me?
I also found the MM20-33366-000 from Knowles, with specs that may fit my need. Unforntunately there are no breakout Boards for this MEMS.
Thank you!