Hi,
I am putting together a micromod setup for some tasks. Can someone tell me if the attached are compatible and have good software support? The qwiic stuff I can’t imagine is a problem though it would be good to get confirmation that the STM32 is fast enough to drive the display.
Mostly this probably boils down to asking: is the Ethernet board is compatible / supported with the STM32 processor board? Will the PoE function power the main board (even though that is 3.3 and the PoE is 5V output?