Hello,
I am using the Sparkfun Pro Micro along with the mini gps shield and the GP-735. I’ve followed the instructions on the mini gps shield hookup guide but I am unable to get any information from the gps. The first code example in the hookup guide is supposed to display information through the serial monitor. I’ve tried that and I have a long enough usb cable to set the gps receiver in a window sill but it never locks a position and the led on the shield never comes on. I’ve also tried the second example code in the hookup guide and went outside with a clear view of the sky, still nothing. I have a micro sd card and a 5V rechargeable battery pack that I use with with my full size usb logger shield and Uno so I know that those two components work fine. In both cases I have let the board run for several minutes at a time.
I found a post on here (Pro Mini GPS Shield - TinyGPS++ error) about someone else having similar issues. I installed an older version of the IDE (1.0.5) as recommended and still no luck. I know that I am uploading the sketch to the board just fine as I am able to tweak the serial monitor output, just the text it displays when there are no satellites found.
Is there some way I can test to see if something is wrong with either the shield or the GP-735? I’m not a professional when it comes to all of this stuff but I did manage to build the full size version of this as I mentioned above and have used it for well over a year now with no issues.
Thanks,
Andy