Molex part number for pin that fits test probe

There is a molex receptical pin that crimps onto a wire that fits perfectly onto meter test probe, does anyone have a part number or series number for them? I have some high power load resisters for testing outputs. I intend on soldering a second set of wires to the resistors and crimping these pins onto the ends of the wires so that if I want to attach a meter to monitor the voltage it will be simple and quick. I used to know the part number for this part and am unable to find it.

If you want help you need to provide more information.

Which test probe? Do you have a reference number? Do you have pictures?

This was a long shot post. The test probes are whatever test leads come with a standard Fluke 179 meter. Somehow I think those test leads are standard across manufacturers. The Molex product I have in mind was intended to go in a nylon plug but fits a DMM probe as if it were made for it. I have used them in a previous employment experience and recently seen a picture of someone doing this but cannot recall where I seen the picture. The way it is used is the recepticle is crimped onto a wire then heatshrink is applied over it. Makes an awesome way to securely hold a meter probe.