What is that connector on PRT-00091?

PRT-00091 is described as “Classic 9V snap connector terminated with 2-pin polarized Molex connector with 0.1” spacing. The cable is 26AWG and is 5" in length."

However, the exact Molex part number isn’t given, so I am at a loss as to which on-board connector to order for it. While I suppose that any 0.1 inch male header will work as a kludge, I would really prefer a nice, mating, polarized jack for it.

Can anyone help?

Hi bobcruz,

The connector on the 9V Snap Connector mates really well with our [Polarized Connector - Header (2-pin). The photo for that line of products is a bit confusing since it shows different types of headers and housings but I just tested this with our stock and the 2-pin connects perfectly with the 9V Snap Connector.

I hope this helps you find the right part!](Polarized Connectors - Header (2-Pin) - PRT-08233 - SparkFun Electronics)

@TS-Mark,

Thank you for your prompt reply, and the useful information.

I would, however, suggest that you provide a link to the matching jack on the page for the battery clip+lead. You’d save your customers some frustration, and sell more product!