If I wanted to upgrade the screen as it’s super small. What options do you sell that would work with the Qwiic interface. I have some larger Nextion screens. Assuming that I am powering them separately as they take 5v in the larger screens. Going to experiment with the TX, RX off the ESP32 breakout and see if I can get these working with Nextion (with a 5v supplied seperately.
Our largest Qwiic enabled screen is the 1.3" OLED that is already in the RTK mosaic-X5, so we don’t have a good upgrade option, sorry. Additionally, the firmware is written to expect the 1.3" pixel layout so adding a different display will require firmware work. But that’s the beauty of open source! Please hack away! The firmware is here.