yelw0rc  
                
                  
                    September 28, 2020, 12:18pm
                   
                  1 
               
             
            
              Hello,
I have problems with the MP3-Shield getting a sound out of it.
That’s my second Shield I orderd, because I thought I damaged the
first with wrong wireing.
I use the Shield with an Arduino Uno board.
I guess everything is working, but I can hear no sound over headphones.
The headphones were tested with other devices and they are ok.
I use the example sketch “FilePlayer”. When I open the serial monitor
I can hear some quiet crackle over the headphones. When I start to play
an audio file, I can’t hear anything. I used the “+” for turning up the
volume with no difference. When I use the “d” or “l” option for listing
the audio files on the sd-card, all files are shown. When is use the “S”
switch, it tells me, that an audio ist still playing, but with no
outcoming sound. I have the same problem with both boards.
What I’m doing wrong and what can I do to make it working?
Thanks for help.
Greets
yelw0rc
             
            
              
            
           
          
            
            
              Hi yelw0rc.
We test these shields during manufacture so you should have received a working shield.
What size SD card are you using? You might try a different brand card and use a card that’s 16GB or smaller in size.
If you’re still having trouble after trying that, send a photo of the top and bottom of your shield so we can take a peek.
             
            
              
            
           
          
            
              
                yelw0rc  
              
                  
                    September 28, 2020,  5:26pm
                   
                  3 
               
             
            
              Hi TS-Chris,
thanks for your answer.
After hours and days working around with two MP3-Player Shields, testing different sd-cards without positiv results,
it came to my mind to try another Arduino Board from another project. What shell I say … the Arduino was the problem.
After useing another Arduino, it worked like a charm. Both Shields :roll:
I have another question to an expert.
What do I need to use a 0,5w or 0,25w 8-Ohm speaker with the shield?
Thank you vervy much and greets
yelw0rc
             
            
              
            
           
          
            
            
              
What do I need to use a 0,5w or 0,25w 8-Ohm speaker with the shield?
 
You may be able to directly drive a small speaker from the audio output pads on the shield, but the volume may not be that much. You’d have to give it a try and see if it’s loud enough for your application.
If it’s not loud enough, a small amp like the [Noisy Cricket  would do the trick.](https://www.sparkfun.com/products/14475 )