Hi all,
I’ve recently started working with an Arduino for a project of mine and have reached the point where I’d like to incorporate sound. I came across both the MP3 Trigger and the MP3 Player Shield, but I’m not entirely sure which one is better suited for my project since I’m still new to all of this. As for what I’m trying to do for the sound, I have an IR remote and when I press a button on the remote I’d like the corresponding sound effect to play. So I press button “1” sound effect 1 plays, press button “2” sound effect 2 plays, so on and so forth. So any advice/help on whether the Trigger or the Shield is better suited for my project would be great.
Thanks!