Hi, I’ve recently bought an Arduino Lilypad that I’m brogramming with “FTDI Basic Breakout - 3.3V”. I’ve done this before without any problem, but with this new one arduino it’s not possible. Here’s the output when I send the sketch in debug mode:
Binary sketch size: 920 bytes (of a 14336 byte maximum)
/home/ubuntu/Desktop/arduino-0018/hardware/tools/avrdude -C/home/ubuntu/Desktop/arduino-0018/hardware/tools/avrdude.conf -v -v -v -v -patmega168 -cstk500v1 -P/dev/ttyUSB0 -b19200 -D -Uflash:w:/tmp/build4700057582393089853.tmp/Blink.cpp.hex:i
avrdude: Version 5.4-arduino, compiled on Oct 22 2007 at 13:15:12
Copyright (c) 2000-2005 Brian Dean, http://www.bdmicro.com/
System wide configuration file is “/home/ubuntu/Desktop/arduino-0018/hardware/tools/avrdude.conf”
User configuration file is “/home/ubuntu/.avrduderc”
User configuration file does not exist or is not a regular file, skipping
Using Port : /dev/ttyUSB0
Using Programmer : stk500v1
Overriding Baud Rate : 19200
avrdude: Send: 0 [30] [20]
avrdude: Send: 0 [30] [20]
avrdude: Send: 0 [30] [20]
avrdude: ser_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
avrdude: Send: Q [51] [20]
avrdude: ser_recv(): programmer is not responding
avrdude: stk500_recv(): programmer is not responding
I think I could upload the Blink example for the first time, but now I don’t know if the led in pin 13 is blinking because of the bootloader or because of the Blink code.
Any Idea?
Thanks