I’ve just finished laying out my first board and thought I should let the more experienced have a quick look.
It’s a pretty basic board that has an atmega168, a current sensor (ACS712-20A), and a relay. It will be used to automatically turn on a second machine (the slave) when my board detects current being drawn by another machine (the master).
Since it’s going to be controlling mains (up to around 10A), I would like some feedback regarding the width of the traces for the relay.
Here’s my schematic and board:
http://www.mediafire.com/file/ad5midzto … witch2.sch
http://www.mediafire.com/file/natymzimd … witch2.brd
(The specific mosfet I would like to use is the “BSS138”, since I have a bunch of them already. The relay is the Omron “G4A-1A-P-E-DC12”.)
Any comments/advice is greatly appreciated. 
EDIT: I have just been going over my design and I’m not sure if the mosfet is under spec’d. It is rated for max 200mA, and my relay will draw a nominal 75mA, but I don’t know how accurate that is.
Would I be better getting a slightly larger mosfet, since I’d also be able to use it for other circuits as well? Any suggestions on which one? (I’ve never used mosfets before, so I don’t know what the “usual suspects” are…)
Oh, and I also noticed the footprint for my relay is wrong. Lucky I noticed it now