My order seems to have been forgoten or stuck???

My order seems to have been forgoten or stuck???

Order Number: 10085

Order Status: Processing

Panel: 548

Created On: 2009-10-26 16:32:21

Last Changed: 2009-10-27 10:28:39

Completed On: Order Not Yet Completed

Tracking Numbers: No Tracking Number available

Notice how that pannel should have been sent but it still says processing does that mean it is being made or that sparkfun or their system coughed on my files?

This is only an estimation of how future panels will be filled based on the order queue. Actual panels may vary.

Last design ran was number: 18545

Last panel sent out for processing was 550 on 10/29/09

Last panel shipped was 536 on 10/27/09

The line for the DRC Bot has 0 people waiting.

batchpcb was very helpful they fixed my holes in my board being too small and saved me from having coasters.

Thanks guys the problem will not happen again and I have 5 more boards that are all different to send to you soon.

I also hope to have some kicad tutorials in instructables soon after I am done with this process so others can see.

When your board is on a panel, it is set to processing. Until I receive it from the manufacturer the status will remain that way until it is shipped out. Which is usually less than a hour from when I receive it.

-Patrick

Yea my board is in the status where it is comming to me. Thanks after I test this one I will make some more orders.