Hi there,
I’m working on an interactive sculpture project which involves 10 distance sensors VL53L4CD - see attached drawing. I distribute the data/power using a couple of mux boards in daisy chain and I extend the system using endpoints and 3m ethernet cables.
I’m wondering whether the power outputted by the dev board (SparkFun Thing Plus - Artemis) is sufficient to power the 10 sensors especially with the voltage drop resulting from the mux boards + 3m ethernet cables.
The only thing I know is that the VL53L4CD has a max consumption of 24mA. Do I need to inject power?
If so, the first endpoints look like an option (see exemple of power injection on the drawing). What do you think?
Many thank!
Tom