Need help with choice of items for RTK project

Hi,

I have a drone whose flight control software runs on a RPi 4. The drone itself has GPS & RTK receivers/antennas on the rear 2 of 4 motor arms. The issue is that the RTK update rate is too slow for my requirements, so I wanted to supplement it with a RTK breakout or pHAT board using the Mosaic-x5 or the ZED-F9P or the LG290P.

My questions are that with either the breakout or the pHAT boards, with a 3-band Helical antenna:

(1) how easy is it to get the RTK coordinates from either the USB or Serial ports?

(2) How easy is it to minimize signal interference with 3-antennas on the drone.

I was thinking of starting with the LG290P breakout board and then if that works with RTK, I would get the Mosaic-X5 board with the higher update rate. All of my code is in C/C++ and I have written code to work with serial ports, but my experience is limited. Any help is appreciated.

Cheers,

-atin

Very Easy…that’s how most function out of the box :slight_smile:

The GNSS antennas don’t produce any interference.
The ESC’s and motors on the Quad produce EMI (noise), but adding a 3’rd antenna doesn’t add any noise.

If (by chance) you want a higher update rate for EXIF data on photos, you might have better options than adding another RTK System. But obviously I’m just guessing at what’s driving that requirement :wink:

Thanks Ryan! I was referring to the RTK update frequency.

| rftop Regular
June 6 |

  • | - |

atin_kothari:

(1) how easy is it to get the RTK coordinates from either the USB or Serial ports?

Very Easy…that’s how most function out of the box :slight_smile:

I need it to be via some API, so that I can get at it programmatically.

atin_kothari:

(2) How easy is it to minimize signal interference with 3-antennas on the drone.

The GNSS antennas don’t produce any interference.
The ESC’s and motors on the Quad produce EMI (noise), but adding a 3’rd antenna doesn’t add any noise.

If (by chance) you want a higher update rate for EXIF data on photos, you might have better options than adding another RTK System. But obviously I’m just guessing at what’s driving that requirement :wink:

I guess I’ll just have to try it out with the helical antenna.

Cheers,
-atin

I’m a big fan of the PostCard when incorporating RTK into a device or product. With it’s onboard ESP32 - it’s easy to configure the PostCard to output whatever you need.

The product page claims up to a 20 Hz Update Rate, but that feels optimistic, to me :wink:

image
It might make 20 Hz… I’ve honestly never tried.

I have tested close to 10 different models of Helical Antennas with the PostCard.
I was pleasantly surprised with the repeatability of most, if not all…given the tiny size of those lil critters.

Thanks Ryan!

The postcard is backordered, so I got the breakout & helical antenna only. I’m looking at bluetooth/wifi boards. Basically, I need all of this to work with my program on a Raspberry Pi. Ideally the update will be 50 Hz, but for now 10 Hz should suffice for testing.